Part Number: ADS7138-Q1
Other Parts Discussed in Thread: ADS7138, ADS7128, BP-ADS7128
Hello team,
My customer has use the ADS7138-Q1 in their ADAS system in A sample, while they are waiting the board, they want to use the EVM board to start the software development.
I notice that there is only ADS7128EVM board with ZCD and RMS function, so can they use ADS7128EVM board to do the software development?
Please help evaluate the 2 solutions, give us feedback and recommended solution.
1. One solution is that replace the ADS7138 in the ADS7128EVM board:
- Can these 2 sockets do the replacement just for the software development?
- Any spec difference between ADS7128 and ADS7138?
2. Second solution is that use ADS7128EVM board for convenience:
- I notice that the register difference between ADS7138 and ADS7138 as below.
- Aimed at 0xF, 0xC0/1/2, 0xE3/4/7, Can ZCD and RMS disable and how to disable?
- Aimed at the 0x11 and 0x16, what the difference between the 2 sockets?

Thanks,
Lanxi Li