Other Parts Discussed in Thread: ADS7066
I am using the evaluation board of ADS7066, and when I connected it to a signal generator and tried to drive a DC voltage, I got non accurate measurements at the GUI.
the left column is the voltage that I set at the signal generator, and the right column is the voltage that was measured at the GUI.
I am using Model WW2571A of the signal generator.
do you know what might be the reason?
100mV -> 0.1212V
200mV -> 0.3V
300mV -> 0.51V
400mV -> 0.71V
500mV -> 0.91V
600mV -> 1.12V
700mV -> 1.32V
800mV -> 1.523V
900mV -> 1.725V
1V -> 1.93V
thanks!