Part Number: ADS1262
I'm currently trying to read four differential sensors using ain0&ain1.....up to ain5&ain6. The first three sensors are working great, but I don't get any reading on ain5&ain6. In the datasheet, it doesn't say those two can be a REFP or REFN. Does that mean they can't be used for a differential sensor input? Is there a setting that could be causing ain5&ain6 to not work the way I'm intending?