Part Number: ADS131M02
Hello,
we are wondering whether the ADS131M02 can be used in the following way:
- interfaced via SPI pins (MISO, MOSI, SCLK, CS), but neither DRY or SYNC/RESET connected
- modulator clock CLKIN generated by dedicated oscillator (not synchronized to anything else)
- global-chop mode or continuos conversion mode
The manual advises to also use DRDY or SYNC or the modulator clock CLKIN (9.1.3).
In our scenario there is no need to synchronize the adc sampling/readout and we would use simple polling. "Losing" a sample is not a problem.
Are the following assumptions correct?
- As there is a FIFO, readouts must be attempted twice. The last conversion data is the most recent (8.5.1.9.1).
- Thanks to the crc, transmission errors can be detected (1 bit only)
- The automatic timeout allows recovery from all interface problems without the need for the SYNC/RESET pin
- It would not be possible to make proper use of the "Standby Mode", because the modulator clock can't be deactivated
Sincerely
JK