Other Parts Discussed in Thread: AFE4490,
Hi all,
I want to evaluate the AFE4490 for a new product application and I am going to buy the evaluation kit AFE4490SPO2EVM.
I need to use an AFE that can output analog signals so that I can sample with the internal ADC of my own MCU.
I noticed that I can use the BYPASS MODE, with analog output voltage that becomes available on two pins RX_OUTP and RX_OUTN.
Now, I would like to use only one single led (IR one) and in a "continous" way, meaning without the 4 phases (as it is by default, see attached figure from datasheet).

I need that only the LED1 is ON for the 100% of the Pulse Repetition (that loses at all its meaning), so that, sampling on RX_OUTP and RX_OUTN, I can read at any times data from PD triggered by LED1 only.
Basically I don't want to have LED 1 ON, LED 2 ON, Ambient 1 and Ambient 2 periods, but only LED 1 ON for all the time of the PR (in this way the PRF becomes meaningless).
Is there a way to set this kind of configuration? I need to know that before completing the purchase.
Thanks for the help, looking forward to read your advices.
Regards,
Alessio