Hi,
We use the ADS7830 for the voltage sampling in our new project, and now we have the below issue for the I2C bus:
1. We use the ARM MCU for the I2C matter and the ADS7830 for the I2C slave, and now, the MCU send out the ADS7830 address and there are no ACK signal feedback;
2. The waveform as below:

3. Based on the above, we send the address signal again, there is the ack signal feedback and the ADC is normal;

4. We test other board, and this issue is only for the first power on, and we consider this is the probability event;
5. And we check our schematic diagram and we have no idea if there are any error, the schematic diagram as below:

6. Plesae kindly review above schematic diagram and share your comment how to solve this issue, thanks.