Part Number: DAC81408
Other Parts Discussed in Thread: OPA2187,
Dear Technical Support Team,
There is Figure 67. Schematic for Remote Ground Tracking on datasheet page 46.
Do you have this accuracy between REFGND PIN and REF PIN?
1kΩ resistor are used in the summing circuit and the non-inverting amplifier. For example, with a 1% non-inverting amplifier, 1+(1.01kΩ/0.99kΩ) or 1+(0.99kΩ/1.01kΩ) would shift 2%, will this also affect the accuracy like 2.5V±2%?
Internal reference range is from 2.4975V to 2.5025V(2.5V±0.1%).
Best Regards,
ttd