Other Parts Discussed in Thread: TSW14J57EVM, LMK04828
Hello,
1,When I set the data rate to 9G , the following dialog box will still be displayed(HSDC pro) .How do I do it?


2,I want to use the "811 mod"of the DACEVM,I don't want to use J4 to connect to an external reference clock. I want to use On-Board VCXO Clock Mode (CMODE4) Like the picture below. I would like to confirm the Settings of these parameters(about On chip PLL、 PLL2 configuration 、Clock Outputs、clocking,etc), as shown in the PPT below h8.docpe.com/Download/021809390957/021809390957.html (by Chase W).