Part Number: ADS1260
hi,
When calibrate(full-scale), I guess the device will change internal channel to reference 2.5V.
This is ok when gain is 1.
But when i set gain to 32, and perform full-scale calibrate, will it give correct result? will it overflow?
will the device generate correct input voltage when i change diffent gain by himself?
Need I provide different input voltage externally to calibrate different gain when i use full-scale calibration?
Best regardings