Hi Team, seeking some support.
Using the ADS7066 for a data acquisition application. I have a MAX41400 amplifier for 10uV-10mV(5Hz-5KHz) signal amplification and this goes to the RC(kickback) filter before the input of the ADC. the value of the RC filter is chosen with the help of Analog Engineer's Calculator app from ti and the values used are 51ohm and 620pF.
I am using two inputs of the ADC; channel 3 and channel 4. And I removed the RC on channel 3 and the signal is much better than on the channel with the RC.
I have attached images from a custom GUI which plots the data(10Hz) and the first image is without the RC filter and the second image is with the RC filter circuit.
As you can see the input to the channel without RC filter is much cleaner than the one with RC. it gets worse as I increase the frequency.
Do you know why this happens? Is it because of the values I have chosen? Or do you think it's better not to use the RC filter or do you think using the right RC filter might again improve the signal being recorded?
Thank you.
-Mark