Part Number: ADS1293
Hello,
I use custom ads1293 board and I have faced a problem. I use lipo battery for the board. I need to calculate battery level and wanted to use feature of the ads1293.
The battery voltage source is connected to the VDD pin. Hardware designed referanced from the datasheet and it works properly. Problem is I can not read ADC value of the battery over FLEX_CH_CN1. I set "VBAT_MONI_CN" register as 0x01 and also set "AFE_SHDN_CN" register as 0x01 too.
According to datasheet of the ads1293 POSx of the FLEX_CH_CN1 register need to be read ADC value of the battery but I always read FLEX_CH_CN1 as 0x00 or last written value. VBAT_MONI_CN and AFE_SHDN_CN resigters were writen and read successfully.
Also when I read ERROR registers value of ERROR_RANGE1 is 0x14 which is "channel 1 instrumentation amplifier negative output near negatice rail" and "channel 1 instrumentation amplifier negatice output near positive rail". Do you thin the error code related the battery monitoring?
Could you kindly please tell me which reason can cause the problem?
Yours Truly,
Ali Serbetci