Part Number: ADS1299-4
Other Parts Discussed in Thread: ADS1299
Hello everyone! The following is the schematic made for recording scalp potentials. In addition to the EEG amplifier, I have made a battery management system (figure 2) that could be used to boost up the 3.7 V of the Li-Po battery to 5 V (Voltage supply - AVDD to ADS1299). The 3rd figure consists of LDOs to maintain a stable voltage supply to the EEG amplifier and other circuitry. Sometimes, I find everything to be working fine but sometimes I notice 22 Hz / 33 Hz and its harmonics in the PSD which are killing my signal of interest. I request the TI community to help me figure out the issue in the schematic.