This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82EVM: In the following Settings, why the output signal quality is poor and the time domain waveform is not visible at all

Part Number: DAC38RF82EVM


1,In the following Settings, why the output signal quality is poor and the time domain waveform is not visible at all?

2,Is the maximum frequency of the waveform in the following imported file calculated as follows: 375M÷4 (4 points per cycle) =93.75M  ?