Part Number: AFE5809
Other Parts Discussed in Thread: AFE58JD48, ADS8900B, ADS127L11
Hello,
I am interested on AFE5809 part to use for sonar application.
I have two main design parameters.
1) 24 bit resolution of ADC.
2) The frequency of interest is 50 kHz -/+ 10 kHz bandwidth.
Is there an available part which can satisfy above design parameters or any design suggestion to meet these parameters
Thank you.