I realize the question has been asked before but reading the various blogs and ADS52J65 datasheet, I just want to confirm that my understanding is correct regarding trace length matching in my particular setup, which matches the JESD204B example in the ADS52J65 datasheet, page 124, figure 158.
I'm using two ADS52J65 JESD204B ADC's in my design, a Xilinx US+ FGPA where I use two GTH banks and a Clock Generator device in a subclass 1 setup in order to achieve deterministic latency using SYSREF as timing signal.
Question 1: Is my understanding correct that based on the system diagram below, trace length matching is required for:
---------------------------------------------------------------------------------------
- The ADC_SYSREF to DEV_CLK signals between the two ADC's.
- The FPGA_SYSREF to FPGA REFCLK1/2 signals BUT there is NO requirement to match FPGA to ADC signals.
- TX_TRIG for ADC1 and ADC2.
- SYNC for ADC1 and ADC2 BUT there is NO requirement to match TX_TRIG to SYNC signals.
---------------------------------------------------------------------------------------
Question 2: ADS52J65 datasheet page 132 states the following for the CML outputs:
- CML traces require a controlled impedance of 100 ohm differential. The routing of different lines must be matched as much as possible to minimize inter-lane skew. However trace length matching is less critical for the JESD interface as compared to LVDS interface.
Is there a practical limit on "as much as possible" when it comes to trace length matching for the CML outputs?