This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3662: Differential Signal Level for CLKP and CLKM

Part Number: ADC3662

Hi,

Good Day.

We need to know the Differential Signal Level for CLKP and CLKM.

Datasheet doesn't mention what is common mode required on the differential clock input.

We need to know the levels of all the differential signals' input and output.

Please advise. Thank you very much.

Best Regards,

Ray Vincent

  • Hi Ray,

    Please refer to pg. 33 in the ADC366x datasheet (8.3.2 Clock Input / 8.3.2.1 Single Ended vs Differential Clock Input) for the differential clock input requirements. For differential clock input - "the clock input can be AC coupled externally. The ADC366x provides internal bias". Figure 8-14 shows the AC Performance vs Clock Amplitude. 

    Pg. 8 of the datasheet shows VID / VCM, but they are listed above the 'Clock Input' parameters which could be why you had trouble finding them. I will check to see if this is a datasheet error. 

    Regards, Amy

  • Hi Ray,

    There is a datasheet sheet error here. The clock amplitude will directly impact the internal aperture jitter. The clock input has a small range threshold to trigger the sampling process. The smaller the clock amplitude, the longer the clock signal takes to go through that threshold - and this timing uncertainty equates to jitter in the time domain. The clock amplitude listed above specifies the device working properly. Please refer to Figure 8-14 for SNR vs. clock amplitude. 

    Regards, Amy