Part Number: ADS7828
Hello,
We are using an external reference of 3.3V. In the datasheet, it is specified that the measurement range is from 0V-VDD when using an external reference. However, we do not read the maximum value of bits (4095) when connecting the input channel to 3.3V. We also do not read 0 when connecting the input to ground. Are we not understanding the datasheet correctly? What is the transfer function from bits to voltage?
Thanks,
Julia