Part Number: ADS9817
Hi,
Customer would like to use ADS9817 for +15V.
Can ADS9817 support AINxP 15V and AINxM GND?
In the datasheet, AINxP max is 14V. Is maximum input 14V?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS9817
Hi,
Customer would like to use ADS9817 for +15V.
Can ADS9817 support AINxP 15V and AINxM GND?
In the datasheet, AINxP max is 14V. Is maximum input 14V?
Thanks.
Hi David,
The ADS9817 can handle +/-12V as its full-scale range, so you will see clipping beyond that. The +/-14 you noted is in the operating voltage range before the over voltage clamp kicks in. You cannot accurately measure +/-15 V without some sort of attenuation.