Part Number: ADC3422
Other Parts Discussed in Thread: THS4551
Hello,
I tested LVDS output data using below sequence.
1) set register 009 = 0x01;
2) set register 70A = 0x01;
3) set register 00E = 0x60;
4) set register 00F = 0x00;
5) set register 00A = 0x11;
6) set register 00B = 0x11;
7) set register 006 = 0x02;
The wire 0 = 000 and The wire 1 = 100 (expectation is 000)
Chang setting
5) set register 00A = 0x22;
6) set register 00B = 0x22;
The wire 0 = 111 and The wire 1 = 011 (expectation is 011)
Chang setting
5) set register 00A = 0x44;
6) set register 00B = 0x44;
The wire0 and wire 1 output same as expectation digital ramp.
Chang setting
5) set register 00A = 0x00;
6) set register 00B = 0x00;
7) set register 006 = 0x00;
Setting input voltage with fixed to 0V.
The output jump with parity about 30~40 count. (expectation should similar value)