This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3442EVM: maximum sps

Part Number: ADC3442EVM
Other Parts Discussed in Thread: ADC3441, ADC3444, ADC3443, ADC3442

In the case of the ADC3442EVM, I know that it has a specification of 50MSPS.

However, in the test setup of the manual, 125M is to be used.

In addition, as a result of checking at 125M, it was found that the measured value was properly confirmed. What is the max SPS?

  • Hi Yuhyeon,

    The ADC344x comes in different speed grades - ADC3441 (25MSPS), ADC3442 (50MSPS), ADC3443 (80MSPS), ADC3444(125MSPS). The users guide uses the 125MSPS as an example. The max speed of the ADC3442 is 50MSPS. 

    Regards, Amy