This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3644: Read and write to the SPI

Part Number: ADC3644

Hello,

I am preparing to read and write to this ADC chip through the SPI interface. But I don't see anywhere in the datasheet (other than the eFuse) that says how long to wait between each command written to the bus. Does it matter, or is the 1ms for the eFuse sufficient for all commands?

Thanks!