Part Number: DAC7641
I have selected a DAC7641 to convert a 3 digit thumbwheel switch to a 0 to 2.99V analog signal. The DAC is powered with a single 5V supply as shown in FIGURE 2 of the datasheet.
- A microcontroller converts the 3 BCD switch outputs (0 to 299) to a 16 bit binary word.
- The binary word is multiplied by 219, i.e., 0 to 65481
- An existing 2.5V reference is used for this and other purposes in this design.
- The Vout of the DAC7641 drives an opamp with a gain of 1.2.
- The changes in the thumbwheel switches occur randomly.
QUESTION: Is there a static setting of the digital interface that will change Vout without changes to the digital interface?