Part Number: TSW14J57EVM
Dear TI,
I got the preliminary version of HSDC Pro 5.30 and tried to use it with TSW14J57EVM. I uninstalled the previous version of HSDC. I get the following error message upon starting the program:
Invoke Node in TSW1400.lvlib:Startup Splash Screen.vi
<APPEND>
VI Path: <b>C:\Program Files\Texas Instruments\High Speed Data Converter Pro\High Speed Data Converter Pro.exe\Frame.vi</b>
and

I have no option to choose the board to connect with (as in the previous version). Do I need to install some drivers or any additional files, or change some existing files?
I am trying to use this version of HSDC to accelerate the process of sampling from my ADC and sending the signal to the PC. I also had issues with get_capture_data (32 bit) - I always got just half of the points and the other half came in as just zeros. To me it seems that the TSW samples from both ADC channels eventhough the configuration states it is one channel only. I therefore use save_raw_data_s_csw to save the sampled data in a csw file and then I read the file on the PC. This works well but is not helping in making the process faster.