This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131M08: Reading samples completely asynchronously (ignoring DRDY)

Part Number: ADS131M08


Hello!  I'd like to ask about the feasibility of reading samples completely asynchronously from the ADS131M08.  For our applications, it would be great if we could just completely ignore DRDY and allow the ADC to free run, then read the latest data from it at arbitrary times.  I found this thread which indicates that this is not possible with the ADS131Ax, but might be possible with the ADS131Mx.

The datasheet states that this ADC has a 2-deep sample FIFO.  When a new sample is read, it is enqueued to the FIFO, and if there are already two samples in it, the oldest sample is dropped.  My question is, what happens if an SPI read occurs at the exact time that a new sample is enqueued to the FIFO?  Is there potential for a race condition, where data is updated in the middle of the processor reading it?  Or does the FIFO have logic to keep a reading in the buffer during an SPI read? 

The datasheet is not very clear about this, so some clarification would be appreciated!

Thanks,

    Jamie

  • Hi Jamie,

    Yes, I've seen these types of questions about this a couple of times now. Funnily enough, I thought I had written something about it already but I can't seem to find the thread. Before I answer the questions directly, here's some old notes I have from our team:

    Note, the device is not design to have a "conversion start" or "single shot" function. As soon as the device powers on, the device starts converting.

    The device has an “output data buffer” and a “FIFO buffer”. Both buffers can only hold one conversion result.

    The data output on the SPI is always from the FIFO buffer.

    In the following examples I use the following notation to indicate which sample is in which buffer [# of sample in output data buffer | # of sample in FIFO buffer]

     

    Example 1:

    When the first conversion (#1) completes it is placed both in the output data buffer and the FIFO buffer [#1 | #1].

    If you read the data right after the conversion completes, then you are reading result #1. The content of the buffers stays at [#1 | #1]. Means you can read out the #1 conversion result again if you would like to.

    Now if conversion #2 completes it is again put into both the output data buffer and the FIFO buffer [#2 | #2].

    If you read the results before conversion #3 completes, you read out result #2 and the buffers stay at [#2 | #2].

     

    Example 2:

    When the first conversion (#1) completes it is placed both in the output data buffer and the FIFO buffer [#1 | #1]

    If the data from the FIFO buffer has not been read and conversion #2 completes, then the output data buffer holds the sample #2 while the FIFO buffer still holds sample #1 [#2 | #1].

    If you read data now before conversion #3 completes, you will first read out result #1. The content of the buffers then changes to [#2 | #2].

    If you read again you will read result #2 now. The buffers stay at [#2 | #2].

    Now when conversion #3 completes it will overwrite the results in both buffers [#3 | #3].

     

    Example 3:

    When the first conversion (#1) completes it is placed both in the output data buffer and the FIFO buffer [#1 | #1]

    If the data from the FIFO buffer has not been read and a new conversion (#2) completes, then the output data buffer holds the sample #2 while the FIFO still holds sample #1 [#2 | #1].

    Now if conversion #3 completes and the FIFO has still not been read, then sample #3 overwrites both the sample in the output data buffer and the FIFO [#3 | #3].

    In this case, both conversion result #1 and #2 are lost and cannot be read anymore.

    Now, onto your questions:

    My question is, what happens if an SPI read occurs at the exact time that a new sample is enqueued to the FIFO?  Is there potential for a race condition, where data is updated in the middle of the processor reading it?  Or does the FIFO have logic to keep a reading in the buffer during an SPI read? 

    I want to confirm, but I believe the output data buffer would be updated as SPI is accessing the FIFO buffer but let me confirm with the team.

    Best,

    -Cole

  • Hi Jamie,

    When a new sample is read, it is enqueued to the FIFO, and if there are already two samples in it, the oldest sample is dropped.  My question is, what happens if an SPI read occurs at the exact time that a new sample is enqueued to the FIFO?  Is there potential for a race condition, where data is updated in the middle of the processor reading it?  Or does the FIFO have logic to keep a reading in the buffer during an SPI read? 

    I've confirmed that the device will wait for the read to finish and then the FIFO will be updated with the new or 2nd conversion (that just finished during the read).

    That being said, if by some chance, another conversion (we'll call it the 3rd) finishes while the read is still taking place (maybe a really slow SCLK?) then the FIFO buffer is updated immediately and the 2nd conversion will be lost.

    Best,

    -Cole