Part Number: ADS1119
Hello.
I use ADS 1119 in several projects and basically the same topology for several projects, recently I'm having a problem when the value of one of the channels saturates to close to 4900mV the value of another channel that is at 900mV starts to vary, I've had a similar problem the one when the value of one of the channels was more negative than the GND, but this is not the case, I already replaced the chip a few times even so after a while it returns to present the same problem.
Other than that, I have some doubts, configuring the ADC as a differential, if the result of the subtraction between two channels is more negative than the GND, can the ADC present a problem?
Thanks