Part Number: ADS1261
I have a question regarding the ADS1261 analog power supply. The minimum recommended value is 4.75 V. We are using a 5 V input and an LDO (LT3042) as the analog supply, however, it could result in voltages around 4.7 V to 4.75 V. I wanted to know if it is all right to work around this minimum recommended VCC or even slightly lower.
Thanks!