Part Number: ADS124S08
Other Parts Discussed in Thread: AMIC110
About 3-Wire RTD Application
Please see the attached file
①Question about power supply
• Digital Supply: 2.7 V to 3.6 V
・Analog Supply: Unipolar (2.7 V to 5.25 V)
In Figure 113. AVDD = 5V
Is there any problem when AVDD=3.3V?
Why is AVDD = 5V set in Figure 113.?
②Questions about 3-Wire RTD measurements
The sensor has 3 wires
Do I need two ADS124S08 to measure two sensors?
③Question about connection of ADS124S08
I need to measure 8 sensors
Is it possible to connect 8 ADS124S08 to a microcomputer?
Can 8 ADS124S08s be daisy chained to a microcontroller?

④Question about connection of ADS124S08
Use AMIC110 as host
Can ADS124S08 and AMIC110 be daisy chained?