Other Parts Discussed in Thread: DXP, DAC81408, DAC81416, DAC80508, DAC8728, DAC8718, DAC8568
I am looking for a 16bit at least 8 channel voltage output DAC.
I want to be able to test with data in a file and stream it and maintain that I can run “indefinitely” at 4khz per channel as part of my testing. It seems that your DXP software would do this. Using your development kit and MMB0 board running DXP on a PC.
Is there some other option that would allow me to evaluate the device? There are other possible DACS, such as
DAC81408/DAC81416 no DXP
DAC80508 no DXP
DAC8728 no DXP
Can you confirm that the setup would be able to keep up with that data rate? (Essentially 4khz x 8 )?
Which option to use? The ones marked no DXP have software but I suspect would not keep up the speed.
There are several options that meet the specs, with some EVMs that mention DXP, some not.
DAC8718 yes DXP
DAC8568 yes DXP
What do I order to get this working?
It appears that the MMB0 is bundled with some kits but not the ones I would need.
Could you tell me the proper part number to purchase along with the EVM?
Should I be concerned about using windows 10/11 with the DXP software
Thanks
Jonathan