Part Number: ADS1014
Other Parts Discussed in Thread: ADS7142
Our application is to monitor laser power. In consideration of signal integrity, ADC would be located closely with transimpedance amplifier,
and the data acquisition module will be 12-15 inches away from a microprocessor.
Several key areas we consider:
1) small footprint of laser monitoring module,
2) low power,
3) less wire connection from the module to microprocessor,
4) ADC conversion sync with laser pulse firing,
5) Laser pulse firing rate is 50 Hz.
6) ADC resolution 12 bit is good enough since we have gain stage at transimpedance amplifier.
Do you think ADS1014 would fit our application situation since it has one-shot mode for achieving the conversion synchronization goal?
If not, do you have suggestion for our application case?
Thanks