Part Number: DAC8741H
With some HART transmitters, we are getting random framing errors. (Roughly 1 % of the times). The modem status register shows 0x4806.
There are still a couple of bytes left (we know this based on the HART frame format) after the framing error which are not coming through the FIFO.
The modem status register does not show CD off for 20 ms more. (Modem status register then goes to 0x4804)
I have two questions:
1. Does the modem stops sending data out after the framing error?
2. Can the modem handle baud rate variation of at least plus or minus 2%