This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8509: Check whether ADS8509IBDW p2p ADS8519IBDBR or not

Part Number: ADS8509
Other Parts Discussed in Thread: ADS8519,

Hi team,

Customer would like to choose the following two ADCs as P2P compatible alternatives, with an input range of ± 10V. However, according to the manual, the circuit connections are inconsistent in this application. They would like to confirm if these two ADCs can be used as P2P compatible sources?

BRs

Hao

  • Hao,

    Yes, both the ADS8509 and ADS8519 have the same pin-out.  There are differences from the standpoint of the internal resistive elements though and the ADS8509 needs the three additional resistors shown above for the +/-10V input range.