This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RF: Source code for "ADCxxDJxx00RF EVM GUI.dll"

Part Number: ADC12DJ5200RF


I'm looking for the source code for the interface dll (ADCxxDJxx00RF EVM GUI.dll)  included in the configuration software for the ADCxxDJxx00RF Evaluation module.

I would like to modify it to work with a board based on the evaluation module with a few modifications.

  • Hi William,

    We are looking into this for you. 

    We will respond by tomorrow.

    Regards,

    Rob

  • Hi William,

    See the link below to download the DLL you requested.

    Please advise, this is a courtesy to our customers and we cannot support any further questions regarding the DLL.

    You are receiving this "as is".

    Regards,

    Rob

    https://tidrive.ext.ti.com/u/r8T3EbTE93i9xPcW/12e60e89-2a87-4c3e-bb83-80889c8a9106?l

     

    The access code is X5r^A9kX

  • Rob, 

    Thank you for the prompt response.  I looked over the labview source,  I am a LabView neophyte, so I apologize in advance if this is a newbie question.

    The source code includes the full EVM GUI application, but I did not see the source code for the specific dll I was looking for. The archive you sent includes the actual compiled dll, but I did not see the source code to create it.

    What I am looking for is the source for this dll:

    ADCxxDJxx00RF EVM GUI\Shared Library\ADCxxDJxx00RF EVM GUI.dll

    The "Shared Library" folder contains the DLL, the associated .h and .lib files., and a "SubVis" folder

    Is the source for this dll available?   I suspect this was created in either LabWindows or Visual Studio, but that is only a guess.

    Kindest Regards,

    Bill

  • Hi Bill,

    Let me check again, sorry about that. I was told it was all in there.

    Anyway, give me a day or two to get back with you.

    Thx,

    Rob

  •  Hi Bill,

    Here is what I heard back from our third party vendor on this. 

    Unfortunately, it doesn't seem to help much. 

    Regards,

    Rob

    The DLL mentioned by customer (ADCxxDJxx00RF EVM GUI\Shared Library\ADCxxDJxx00RF EVM GUI.dll) is a LabVIEW built DLL.

    The DLL contains the functions representing each VI present inside the folder “\ADCxxDJxx00RF EVM GUI\Shared Library\SubVIs". The DLL is built using the ADCxxDJxx00RF EVM GUI.lvproj file under Build Specification section.

    The VIs inside the SubVI folder mentioned above should be the source code you are looking for.

  • Rob,

    On the contrary, it is quite helpful.  Unfortunately, it does confirm my lack of experience with Labview.  I believed the SubVIs were simply wrappers around the DLL.  Clearly, I need to reach out to some of my more familiar colleagues.

    I very much appreciate your help.

    Kindest Regards,

    Bill