Part Number: ADC128S102-SEP
Other Parts Discussed in Thread: ADC128S102
Hi,
Could you check expected error case with abnormal ground?
When 3.3V or 5V is on GND, damage of ADC128S102 is expected according to the datasheet absolute maximum.
The question is
Can this abnormal GND effect to other component around IC like single-ended input or SPI output or VA or VD? even though 3.3V or 5V is on GND, GND is not shorted to VA or VD.
if there is pspice model of ADC128S102 or other similar device, please provide it.
Thanks.