This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1258-EP: Internal System Readings in Autoscan with Chop Enabled

Part Number: ADS1258-EP
Other Parts Discussed in Thread: ADS1258

Hi,

I am using the ADS1258-EP in Auto-scan mode (using Start pin for conversion). I set the CONFIG0/CONFIG1/MUXSCH/MUXDIF/MUXSG0/MUXSG1/SYSRED during initialization of the system in which I am using the CHOP function (CHOP=1). I would like to get the Internal System Reading particularly the GAIN reading. In the datasheet, it indicates that you need to set CHOP=0 prior to taking the GAIN reading. I was wondering if the ADS1258 automatically sets CHOP=0 prior to taking the reading in Autoscan?

Thanks