Other Parts Discussed in Thread: TX7316
How many MHz transducers are suitable for using the TX7316EVM with a center frequency? Do TI have recommended center frequency parameters?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The TX7316 device bandwidth (max frequency support) depends on the transducer load (load capacitor) and the voltage of operation. The 20MHz number mentioned in the datasheet is for a 220pF load with supply of +/-100V. If the transducer load is higher, the bandwidth will be lower and vice-versa.
Regards
Savyan