Hi team,
Confirm two simple pieces of information:
(1) Whether the detection voltage range of the chip is the following information?

(2) Is there flag bit for 12bit data?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Confirm two simple pieces of information:
(1) Whether the detection voltage range of the chip is the following information?

(2) Is there flag bit for 12bit data?
Hi Alan,
(1) Whether the detection voltage range of the chip is the following information?
Yes, those are the input voltage ranges the ADS1015 can support. The full-scale range is configured by bits PGA[2:0] in the Config register and can be set to ±6.144 V, ±4.096 V, ±2.048 V, ±1.024 V, ±0.512 V, ±0.256 V.
Single-ended input voltage signals can range from 0 V up to positive supply or +FS, whichever is lower. Negative voltages cannot be applied to these devices because the ADS1015 can only accept positive voltages with respect to ground. The ADS1015 offers a differential input voltage range of ±FSR. Single-ended configurations use only one-half of the full-scale input voltage range.
(2) Is there flag bit for 12bit data?
The ADS1015 features a programmable digital comparator that can issue an alert on the ALERT/RDY pin.
The ALERT/RDY pin can also be configured as a conversion ready pin.
Hope this information helps.
Best Regards,
Angel