What are the specifications for an analogue signal generator to be used as a clock in the ADS42LB69EVM?
Would the RIGOL DSG815 be a good solution?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the specifications for an analogue signal generator to be used as a clock in the ADS42LB69EVM?
Would the RIGOL DSG815 be a good solution?
Hi Spilios,
The requirement for clock input on this ADC itself is in the datasheet and can be either a single ended or differential sinewave input between 0.3Vpp and 1.6Vpp (differentially). This clock input must be AC coupled. On our EVM, we have the clock input SMA (J3) pass through the balun (T5) to convert to differential signal. The requirements for this input will be approximately (0dBm - 15dBm) or so. We recommend to always use an RF analog signal generator to achieve best performance. Using the Rigol arbitrary waveform generator you list above will not yield best performance of this device as these waveform generators will typically have much worse phase noise/elevated output jitter, which is directly proportional to the maximum attainable SNR of the data converter. The EVM will work if the level is satisfactory but note that the performance will be degraded from the specified values in our datasheet.
Thanks, Chase
Hi Chase,
the RIGOL DSG815 is an RF signal generator, not an arbitrary waveform generator.
Thus if I understand correctly any RF signal generator that can provide at least 15dBm will be ok for my application.
Thanks,
Spilios
Hi Spilios,
Understood. I hadn't searched the model number to find that out and assumed it was the AWG. It will certainly work. I'm not sure on the performance of this signal generator (as compared to something such as a Rohde & Schwarz SMA100A) but functionally, it most certainly will suffice for your evaluation.
Thanks, Chase