Part Number: ADS1292
HI, Staff
Two ADS1292 are used in parallel connection.
Unexpected data is read when reading data at 500sps.
I would like to check if there are any mistakes in understanding in the basic operation
Data sheet of ADS1292 Let me confirm with the circuit of Figure 34
The circuit configuration is the same as Figure34.
・Set Device0 to Master and Device1 to Slave.
・Dveice0 CLK setting CLKSEL PIN = High, CONFIG2.CLK_EN BIT = 1
Set Dveice1 CLK setting to CLKSEL PIN = Low, CONFIG2.CLK_EN BIT = x
・Sampling: 500SPS CLK: 512kHz
Q1: Please tell me the frequency required for SCLK.
I can't understand the meaning of page49 formula (9).
Q2: Since the master uses the built-in CLK, set the CLK pin to output (pin: 17)
Is there any problem connecting the Master's CLK output to the Slave's CLK input (pin: 17)?
Q3: You can judge whether the master is ready for data by observing the DRDY terminal.
How do you determine whether data is ready on the Slave side?
(Because DRDY of Slave is not connected to MCU)
Q4: Regarding data read, Master 72Bit Data → Master DRDY (Master → Slave 72Bit Data → xxx DRDY
Is it OK to recognize that it will be a Read sequence like the one above?
Q5: Is it OK to recognize that CS is set to Low only when accessing each device
(alternately set to Low, never set to Low at the same time)?
best regards
cafain