This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8201: ADS8201 - Unable to read second byte

Part Number: ADS8201

Hi,

We have setup the ADS8201 to read a voltage difference across a differential pair. 

I can set and read all the registers without issue. However when I read the 3 bytes from the ADC channel I get the first byte correctly, occasionally one bit from the send byte but almost always missing any of the last 3 bytes, but I can read the channel address (3rd byte) correctly. 

The sam happens if I switch out of differential pair mode and read channels 1 & 2 independently. 

What am I doing wrong. It feels like I'm reading too quickly after requesting the conversion, but no amount of delay has helped.

I'm concerned I may also be in the wrong SPI mode, there is some discussion online that suggests reads need to be in SPI Mode 1 to write the address I want then switch to Mode 0 before pulling the data. I've tried that, but there was no difference. Incidentally why does anyone design a chip to use different modes for read and write !! 

Any recommendations would be useful.

Thanks

Will