Hello, I use a high speed ADC ADS2807 in my anolog & digital system and I choose DC-Coupled Differential input mode as the image shows. According to my calculation, the Vin range is only -0.375~+0.375 in this circuit. Obviously, this input voltage range is so narrow that it can be exceeded easily and do damage to ADS2807. So I'm looking for a way to protect the chip. Thank you !