Part Number: ADC12DJ5200RF
Other Parts Discussed in Thread: LMK04832, LMX2594
Hi Team,
I am Saisri, I am using ADC12DJ5200RF in my design and it is interfaced with Kintex Ultrascale FPGA using JESD204B protocol.
1. The receiver is not asserting the sync signal when the ADC is configured with the JM3 with 9.6Gbps lane rate, 4.8GSPS sampling clock and four consecutive K28.5 characters are received on each lane.
2. Sync from the receiver is not stable when ADC is configured with JM11 with 3.2GSPS sampling clock and also K28.5 characters are not received properly.
LMK04832 is being used for Rx Core clock and Sysref to both ADC and FPGA.
Sampling clock is generated from LMX2594.
Please let me know if you need any other information.
Looking forward to hear from you.
Thanks.