Hey,
Just want to confirm the LVPECL clock input levels.
Also, what are the AC coupled LVDS clock input levels (figure 35)? If I understand correctly, 0.8V - 1.6V per "LVDS INPUTS: DIGITAL INPUT DATA" section
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey,
Just want to confirm the LVPECL clock input levels.
Also, what are the AC coupled LVDS clock input levels (figure 35)? If I understand correctly, 0.8V - 1.6V per "LVDS INPUTS: DIGITAL INPUT DATA" section
Cameron,
The LVPECL differential voltage needs to be at least 200mV and typical 1V. The LVDS inputs are typically 200mV differential swing with a common mode voltage of 1.2V.
The LVDS INPUTS: DIGITAL INPUT DATA section in the data sheet is for the digital data lines D[9..0], not the input clock.
Regards,
Jim