Part Number: ADS1278
Hello E2E Experts,
Good day.


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1278
Hello E2E Experts,
Good day.


Hello,
Thank you for your post.
The antialiasing filter is not intended to scale the analog input voltage. Any signal conditioning (i.e. gain, filtering, etc.) is typically achieved in a separate section of the input signal chain. You can consider using a fully-differential amplifier like the THS45xx family to drive the input signal to the ADC while also scaling amplitude to +/- 2.5 V.
These FDA devices can also be used to set the input common-mode voltage of the ADC input pins. The ADS1278 expects a typical common-mode of mid-supply (i.e. 2.5 V). There is an internal common-mode pin (VCOM) which can be externally buffered and connected to the FDA VOCM pin. See Figure 87-88 for example.
You may need to adjust your layout design rules according to the recommended layout information in the data sheet. Figure 93 shows the recommended thermal patch etch and via land pattern for the ADS1278 HTQFP-64 package. There is also additional land pattern information at the end of the data sheet.

Regards,
Ryan
Hello Ryan,
Good day.