Part Number: ADS1260
Customer found an abnormal behavior on the register value of temperature sensor at 25degree ambient temp during operation. Here is reading value.
Register value: 14000
Temp value: -59.6degree
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1260
Customer found an abnormal behavior on the register value of temperature sensor at 25degree ambient temp during operation. Here is reading value.
Register value: 14000
Temp value: -59.6degree
Hi Dale, thanks. Since customer connecting bias power of ADS1260 to 3.3V power on AVDD, it would violate the d/s condition. We're just wondering to know if it would cause this fault. In the meantime, we're still asking customer to do the test with 5V power.
Hi Brian,
Violating the datasheet can definitely lead to a wrong result. Once you are able to provide more information, I can help the customer identify it.
Regards,
Dale