Part Number: ADS8674
Hi, i have been testing this ADC to measure the analog input of a channel,
the issue is that when i send a MAN_Ch_n command to read the analog input channel 1 it pretty much always gives me the
same binary data. Even when there is no input in the channel.
see images below
The first image is the Serial Data input of the ADC
The second Image is the serial data output of the ADC
green mark is the clock signal.
in both cases there is nothing connected to the channel analog input
why is the ADC giving me this result if i dont have anything connected to the channel input?
Thank you