Part Number: DAC43608
I have attached an image.

①This is about the setting of the A0 connector.
The DAC 43608 switches addresses depending on which signal is connected to the A0 connector.
Is there any problem with a circuit configuration that branches from the A0 terminal to each terminal and switches between mounting and not mounting resistors on each board?
The structure is as shown in the attached figure.
The SCL/SDA signal is a branched signal that also connects to the EEPROM, as shown in the figure.
②It is also relevant to question No. 1.
When switching the connection to the A0 terminal with or without a resistor, is a resistance value of 0 (ohm) OK?
If you have a recommended resistance value, please let me know.
③If the signal input to the A0 pin is misdetected due to noise, and it is detected to be none of AGND/VDD/SCL/SDA, how does it behave?
Thank you and best regards,