Part Number: TX7316EVM
Other Parts Discussed in Thread: TX7316
Hi Team, seeking some advice.
Trying to generate pulse signals through the evaluation board. However, no matter what we set in the Profile Configuration, the board just outputs nothing (shown in the attached figures, I try to generate 2 cycles of 5 MHz signal).


If we choose the Quick Setup for 5 MHz, we did observe the corresponding (although the frequency is lower than 5 MHz). Therefore, we are thinking the power source and connections should be okay, but there might be some requirement for setting up the pulse signal in the software which we cannot find the related instructions in the files from the web. It looks like only the common patterns settings can work as I did see changes when I change the REPEAR_COUNT. I'm wondering what else shall we change if we want a different pulse length and cycle numbers.

Thank you very much in advance.
-Mark