This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM98725: CMOS OUTPUT

Part Number: LM98725

I have one Question. I am using CMOS ouput. 
Look at the picture.
Yellow is PHIA1, Blue is SH2 (ADCCLK) , Red is DOUT4, Green is DOUT7. 
CIS SP(Start Pulse) is PHIB1, CIS CLK is PHIA1. 
[Page 8, ADDR 0x00, [6] Bit is  0] , [Page 8, ADDR 0x01, [6] Bit is 0]
This picture is PHIA1(Yellow) ,B1(no measure) off.
Is it normal to output from DOUT at this time? 
All channels in DOUT come out the same.
I think it's normal that there is no output. 
Please give me an answer.
Bset regard
SeongHyu Shin.