Hello,
I use a ADS2807 in my FPGA based analog & digital mixed system, but it doesn't work normally. I choose DC-Coupled ,Differential Driver circuit befor the AD input side just as the schematic shows. The chip's temperature rises to about 50° no matter I give it a clock or not (ADS2807's power consumption is about 720mW) only about 1 minute after it is powered. Sampled data is almost totally wrong no matter I give it AC or DC signal, though the DV(DataValid) pin's output wave is correct (about half cycle fall behind input clock). I wonder if the chip have already been damaged or my operation or circuit have some problems.