This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60004: Parallel operation with two dac

Part Number: DAC60004


Dear Technical support team,

I am considering how to operate two DAC60004 in parallel.
Is it possible to use the following without using Daisy Chain Mode?

-Connect individual SYNC_B control signals to two DACs.
-Prepare one pin for receiving SDO. Connect this to 2 branches for 2 DACs.


Is it possible to READ SDO from the DAC selected by SYNC_B using the above 3 pins?

I expect the SDO of the DAC not selected in SYNC_B to be HiZ.

Best regards,

ttd